Browse FAQs

What is the maximum number of implicit connections supported on the BMENOC03x1 module?

Published date: 30 December 2019

Issue
Need to specify the maximum number of IO Scanner connections supported on BMENOC03x1 module configured through the Unity DTM browser.
 
Product Line
Modicon M580
BMENOC0301
BMENOC0311

Environment
ODVA Ethernet/IP 
Unity DTM Browser
 
Resolution
The M580 Ethernet modules BMENOC03x1 supports a  maximum of 128 devices or Implicit client connections (Shared by EtherNet/IP and Modbus TCP) setup/configured through the DTM Browser


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.