{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
My M221 (or M241 or M251) is connected by USB and it does not answer at address 90.0.0.1…
This is a normal behavior: previous controllers as ATV IMC or M258 were seen as modems by Windows, with IP address 90.0.0.1.

This is not the case of M221, M241 and M251: they are seen as generic USB devices and they do not have an IP address when connected via USB.

Schneider Electric Global

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: