Browse FAQs

How can I connect a Magelis HMISTU to a Zelio Smart relay?

Published date: 30 October 2019

The Magelis HMISTU (655/855) can communicate to a Zelio Smart relay via Modbus serial or Modbus/TCP (Ethernet).
 
For serial communication you would need the the following.
XBTZ9980 cable 2.5m or the ZBTZ9982 10m
SR3MBU01BD Zelio Modbus module
 
For Ethernet communication:
Ethernet cable
SR3NET01BD Zelio Ethernet module.
 
Both Zelio communication modules are compatible with the SR3B***BD smart relay only.
  

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.