Browse FAQs

What is the purpose of the M580 SD card?

Published date: 30 October 2019

The SD memory on the M580 is used to backup the application in the event of a hardware issue. 
The application and data (%MW) on the SD card cannot be accessed via USB or FTP.  

The memory card with backup data can be inserted in a new CPU to load and run the application.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.