{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Power Monitoring Expert - I can't read an custom OPC tag that I exposed using OPC Server Assistant - error is 'ReadingIDUnknown'

Issue

When using OPC Server Assistant to expose custom tags for OPC; OpcTestClient  shows and error 'ReadingIDUnknown'

Product Line

Power Monitoring Expert 7.2.x

Power Monitoring Expert 8.x

Power Monitoring Expert 9.0

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Environment

Using OPC Server Assistant with Power Monitoring Expert Software

Cause

This will happen if you rename a device after you have exposed the custom tag. This happens because the OPC Server Assistant uses the System Name when writing information to IONServicesConfiguration.xml, but the OPC Server looks for the Display Name when exposing the data. Once a device has been renamed, the System Name and the Display Name are no longer the same, thus the problem.

Resolution
To workaround this, it is necessary to manually edit the IONServicesConfiguration.xml file. You will need to remove the entry for your custom tag so that is is the section under the correct device name, i.e. the Display Name. Be sure to make a copy of this file before doing the manual edit in case an error is made.

As an example, here is a snippet of an example of IONServicesConfiguration.xml. In this case, a device was renamed from test.floor7650 to test.floor7650_MSB. Notice how the custom entry, that is bolded, added by the OPC Server Assistant used the original device name, i.e. the System Name:

<?xml version="1.0"?>
<i:IONServicesConfiguration xmlns="http://rddl.xmlinside.net/PowerMeasurement/configuration/IONServices/MeasurementTemplates/1/" xmlns:i="http://rddl.xmlinside.net/PowerMeasurement/configuration/IONServices/1/">
<i:ION>
<i:Src label="test.floor7650_MSB" name="test.floor7650_MSB">
<i:MTR ref="Full"/>
</i:Src>
<i:Src label="test.floor7650" name="test.floor7650">
<M label="IN47 Result" name="IN47 Result"/>
</i:Src>
</i:ION>

To correct this, the snippet above would be changed to the custom tag entry (i.e. the Display Name):

<?xml version="1.0"?>
<i:IONServicesConfiguration xmlns="http://rddl.xmlinside.net/PowerMeasurement/configuration/IONServices/MeasurementTemplates/1/" xmlns:i="http://rddl.xmlinside.net/PowerMeasurement/configuration/IONServices/1/">
<i:ION>
<i:Src label="test.floor7650_MSB" name="test.floor7650_MSB">
<i:MTR ref="Full"/>
<M label="IN47 Result" name="IN47 Result"/>
</i:Src>
</i:ION>

NOTE:  To run the OPC Test client you can refer to the following article: https://www.se.com/us/en/faqs/FA247061/

Schneider Electric Global

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: