What causes Concept error message "-1448 Parameter ‘Continue after’ wrong by GetValueService"?
Published date:
12 July 2019
Issue:
Problem animating online in Concept.
Product Line:
Concept Programming Software
Cause:
The IEC service, which is used to update values for animation, failed due to a fault in the communication between the PLC & PC
Resolution:
Check communications between the PLC and the PC.
Minimize animation. Animate only one to three sections in parallel, including the RDE, LL984 and IEC sections.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.