Browse FAQs

How do you create a .PRZ file in Concept?

Published date: 23 October 2019

Issue:
How do you create a Concept archive file .PRZ

Product line:
All Processors that can use Concept

Environment:
Concept

Cause:
Need to create archive program to send out and import with all the Concept files.

Resolution:
To create a .prz or archive file open Concept without any projects open and under file you will see Archiving, select the project that you want archived and start. this will create the archive project.

Note: Concept is obsolete and recommended to go to Unity Pro. Unity Pro can import your Concept .asc file into the appropriate hardware. For more information contact your local distributor or Schneider Electric sales office.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.