How do you monitor the I/O bus with the Unity Momentum?
Published date:
22 May 2019
Issue:
How to monitor the IObus with a Unity Momentum Processor.
Product line:
All Unity Momentum Processors
Environment:
Ecostruxure Control Expert (formally Unity Pro)
Cause:
Errors on the Interbus network on the Unity Momentum
Resolution:
%SW128.0...15 are for the first 16 Unity Momentum Interbus modules and %SW129.0...15 will display modules 17 to 32 on the I/O bus network.
Also %SW132
Meaning of the different bits of the word %SW132.0 to %SW132.15:
%SW132.0 to %SW132.14: These bits contain a value from 1 to 64, signifying the network position of the module that cannot be reached. For example, a value of 8 indicates a detected communications failure in accessing the eighth module on the network.
%SW132.15:
%SW132.15 = 0 indicates a detected general communication stoppage; for example: no power to the module or a break in its input cable.
%SW132.15 = 1 indicates that communication is possible, but the I/O bus ID received from the module does not match the module type contained in the configuration for that position.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.