{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Does ATV212 S-Flex drive come in a Nema 4 or 4X enclosure?
Issue:
Is ATV212 S-Flex available in a Nema 4 or 4X enclosure?

Product Line:
ATV212 S-Flex, all models

Environment:
ATV212 in S-Flex, all models

Cause:
Does SFLEX-212 come in a Nema 4 or 4X enclosure?

Resolution:
No, the ATV212 S-Flex is available in a Type 1, Type 12, and Type 3R enclosures, but there is no option for a Nema 4 or 4X version.
See the S-Flex manual for details : https://www.se.com/us/en/download/document/30072-451-83/

For other enclosed drive options, please look at our ATV660, ATV960, Altivar Outdoor Drive or custom-built drive panels.

Schneider Electric Global