{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How do you set the PID feedback assignment (PIF) parameter to AI1 on the ATV12 Drives?
Issue:
PID feedback assignment (PIF) parameter configuration to AI1 on the ATV12 drives

Product Line:
Altivar 12, ATV12, Machine Drives

Resolution:
IO menu
AII enter
AIIt (AI1) set this for 0 5-vdc, 0 10vdc or 4 to 20mA

CTL menu
Set Ref 1 channel FR1 to AI Virtual 1 ( Command menu)
Set CHCF to SEP
Set Cd1 to Term

FUN menu
PId enter
PIF Set PID feedback assignment to AI1 ( PID Regulator menu)

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Global

Attachment(s)
Programming manual.pdf [9.6 MB]