Browse FAQs

When did the ATS46 soft start become obsolete?

Published date: 04 October 2019

Issue:
Customer would like to know when the ATS46 became obsolete.

Product line:
ATS46, Altistart 46

Environment:
All models.

Cause:
Determine age of unit, product obsolescence

Resolution:
ATS46 became obsolete in January of 2004.  The current replacement is the ATS48. 
There are some differences that should be reviewed by the customer such as wiring, dimensions and ratings. Refer to this article for details on the differences: https://www.se.com/us/en/faqs/FA175441/
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.