Browse FAQs

Can the ATV32 / ATV320 be controlled in local mode from the display on the drive?

Published date: 11 December 2019

Issue:
Customer wants the ATV32 / ATV320 to be controlled in local mode from the display on the drive.

Product Line:
ATV32 ATV320 Drives

Environment:
All models

Cause:
N/A

Resolution:
The ATV32 and ATV320 can be programmed to use the integral dial for speed control.  However, there is no feature for local Start/Stop control on the front of the drive itself.  Adding a remote HMI keypad (VW3A1101) to the drive will provide RUN / STOP buttons and a dial for speed reference adjustment.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.