{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Does the ATS48 offer a programmable relay for a run status?
Issue:
ATS48 programmable relay for run status

Product Line:
ATS48 Altistart 48

Environment:
All

Cause:
Need contact closure with run command

Resolution:
Yes, R3 is a programmable relay, and its factory default is [rnl] 'motor powered' to indicate run status.



The ATS48 also has 2 logic outputs that can be programmed to indicate the motor is running or several other functions.

Schneider Electric Global