Why is it when I do an export in Vijeo Designer, it saves the project file type as a .HMIX?
When exporting a target in a project, it can only save the type as a .HMIX. When exporting an entire project, it must be done in the Vijeo Manager which will export the project as a .VDZ archive.
Released for:Schneider Electric Global
Explore more
Range:
Vijeo Designer
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.