Browse FAQs

Where can I find the SCCR rating for ATV61 or ATV71 18 pulse enclosed drives ?

Published date: 14 June 2019

Issue:
Where can I find the SCCR rating for ATV61 or ATV71 18 pulse drives ?

Product Line:
ATV61 / ATV71

Environment:

PowerGard 18 Pulse Drives

Cause:
None

Resolution:
PowerGard enclosed drive controllers have a short-circuti current rating of 100 kA @ 480 V (RMS symmetrical).

See Altivar® 61/71 PowerGard™ Class 8839 Type CPD 18-Pulse Adjustable Speed Drive Controllers Instruction Bulletin 30072-451-53 for details.


https://www.se.com/us/en/download/document/30072-451-53/

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.