{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What Communication options are standard on the Schneider drives?
Issue:
Available communication options

Product Line:
ALTIVAR 61, ALTIVAR 71, ALTIVAR 312, ALTIVAR 32, ALTIVAR 212, ALTIVAR 12, ATV600, ATV320, ATV340, ATV900

Environment:
All drives all serial number

Cause:
N/A

Resolution :
The standard communication protocols are Modbus  on all Schneider Drives.  However, on the ALTIVAR 61, ALTIVAR 71, ALTIVAR 312, and ALTIVAR 32, ATV320, ATV340, ATV600, ATV900 CanOpen is also standard. the ATV600 has embedded Modbus Ethernet TCP/IP, The ATV340(E) version and the ATV900 have embedded Ethernet TCP/IP and Ethernet IP as standard.

Schneider Electric Global