Browse FAQs

What is the latest firmware of EGX300 and what is new in it?

Published date: 25 July 2018

Product Line
EGX300
 
Environment 
Firmware
 
Resolution
EGX300 Version 4.461 firmware provides:
Updates:
  • Corrected issue where BCPM/BCM Circuit/Channel Names were not being saved after power cycle
  • Fixed problem where custom devices were not being saved on disk update.
  • Updated PM5000 Energy
  • Updated Sepam 40 Trending
  • Updated Micrologic H Real Time View
The firmware and disk update files can be downloaded from the following link:
https://www.se.com/ww/en/download/search/egx300/

It can also be downloaded from file below V4.461.zip

NOTE: See FA212757 for instructions on how to upgrade the EGX300 firmware.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.