Browse FAQs

Does the M580 support system words, %SW138 to %SW140 ?

Published date: 18 February 2019

Issue
M580 and system words %SW138 to %SW141.
 
Product Line
M580 PAC

Resolution
The M580 PAC does not support the system words, %SW138 and %SW140.
The M580 does support the system words, %SW139 and %SW141 but requires the M580 CPU to use firmware 2.10 IR15 or higher.
These System Words were added to offset the starting address of variables which are accessed by Modbus requests.
This functionality was not supported by the Unity Simulator until Unity Pro version 13.1.


You must set the values of the 2 system words %SW139 and %SW141 using the “Initial value” mechanism. Do not use programming code to set the values. Otherwise, when using the PLC init command or setting %S0 to 1 or downloading an application, the 2 system words are set to 0000 and the behavior of Modbus server is wrong.

Failure to follow these instructions can result in death, serious injury, or equipment damage.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.