Browse FAQs

What is SAFF fault on ATV32?

Published date: 10 December 2018

Issue:
What is SAFF fault on ATV32? 

Product Line:
 ATV32 drives

Environment:
 SAFF

Cause:
 n/a

Resolution:
When the following safety functions are being used on the ATV32:

- (STO) Safe Torque Off
- (SS1) Safe Stop 1
- SLS) Safely Limited Speed

You can check your drive configuration file to see if the have been assigned.

If so please refer to the Altivar 32 Variable speed drives for synchronous and asynchronous motors Safety integrated functions manual.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.