Browse FAQs

What is the part number for the screw and standoff for the Momentum NEF adapters?

Published date: 21 October 2019

Issue:
Momentum option adapter NEF and the part number for the screw and standoff or them to be able to order separately.

Product Line:
Momentum Option adapters NEF

Cause:
Either wrong screws and standoffs or missing.

Resolution:
screw W103851350312
standoff 31006550

Note: The Momentum Processors are obsolete and the Unity Momentum Processors are the replacement but with the Unity Momentum Processors you can not use the Option adapters.

 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.