Browse FAQs

Can the displayed color scheme in a Concept V2.6 project be changed?

Published date: 26 November 2019

Yes, predefined color schemes are selectable using an entry "Color Scheme" in the [Colors] section of the concept.ini file. The concept.ini file is in the C:\windows
folder.

[Colors]
ColorScheme=0

The default is 0 and the range is 0 to 12.   The corresponding color schemes are:



 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.