Browse FAQs

What is the screw size for the Current and Voltage terminal connections on the ION6200 meters?

Published date: 30 August 2019

Issue:
A user requires the information of screw size for Current and Voltage terminal connections on the ION6200 meters.

Product Line:
ION6200

Cause:
A user requires the information of screw size for Current and Voltage terminal connections on the ION6200 meters.

Resolution:
The terminal screws are 6-32 standard screws with wire-catchments washers. The part from Cooper Bussmann is F523/J.
More information on ION6200 meters can be found at the link below:
https://www.se.com/us/en/product-range-presentation/1505-powerlogic-ion6200-series/

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.