Browse FAQs

Is there a way to set an alarm when there is a communication error with Vijeo Designer V6.2?

Published date: 30 October 2019

You can use the @sys:2

When there is a communication packet error or communication timeout the bit is set to 1.  When the communication is good the bit is 0.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.