Browse FAQs

What can cause an OPF or Motor phase loss on the ATV312 drive?

Published date: 11 December 2019

Issue:
Getting a OPF or output phase loss on the ATV312 drive.

Product Line:
Altivar ATV312

Environment:
All

Cause:
Motor power circuit is incomplete.

Resolution:
Troubleshooting Tips
Check the motor connections on T1 T2 T3 and verify continuity phase-phase through the motor circuit/windings.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.