Browse FAQs

Can I change an application password in Vijeo Designer at Runtime?

Published date: 07 November 2019

Issue:
Looking for a way to change user names and passwords during operation on the VIjeo Designer Runtime.

Product Line:
Vijeo Designer Runtime (all versions), Magelis, Harmony, iPC, XBTGT, XBTGK, HMIGTO, HMIGTU, HMIGK, HMISTU, HMISTO

Resolution:
Yes it is possible to change a Vijeo Designer application password during operation within the Vijeo Designer Runtime. You can use one of these object from the toolchest folder in your applicatio in order to change the password during operation. Ensure that the panel where this object is placed is secured and password protected. Ideally, the user group with the highest privelages should only access this panel.


 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.