Browse FAQs

If you lose power on a M340 extended rack, do you lose communication to racks down the line?

Published date: 10 July 2020

Issue
M340 extended rack communication with loss of power

Product Line
Modicon M340

Cause 
Loss of power

Resolution
If you lose power on an extended rack in a M340 system the remaining racks will communicate to the main head rack as long as the physical link is not broken.

Example:
If there are four extended racks in an M340 system and the second rack loses power, racks three and four will still be communicating to the main head rack.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.