Issue
The user wants to check the update/execution rate of a particular ION module
Product Line
ION 7300/7550/7650, PM8000, ION 8600/8650
Environment
ION Setup 3.0
Resolution
This article describes how to check the update rate of an ION module using ION setup 3.0:
The user wants to check the update/execution rate of a particular ION module
Product Line
ION 7300/7550/7650, PM8000, ION 8600/8650
Environment
ION Setup 3.0
Resolution
This article describes how to check the update rate of an ION module using ION setup 3.0:
- Toggle the advanced setup mode in ION setup by holding CTRL + Alt and then left-clicking on the meter.
- Navigate to the desired ION module folder ( in this example, the DNP export modules).
- Hold Ctrl and right-click on the meter to show the following selection menu.
- Select the Read Update Period to display the execution rate screen as shown below.
Released for:Schneider Electric Global