Issue
The installation guide doesn't specify if the ground terminals are internally connected.
Product line
ION8600/8650
Resolution
*Warning: Installation and maintenance of this device should only be performed by qualified, competent personnel that have appropriate training and experience with high voltage and current devices. Failure to follow the instructions / warnings in the Meter Installation Guide can result in permanent damage to the meter, severe injury or death.*
The ION 8600/8650 ground terminal is connected internally to the auxiliary power supply's ground terminal. However, to meet electrical safety standards, the meter must be installed with an adequate chassis ground connection and the auxiliary ground 'G' terminal must be connected to earth ground.
The installation guide doesn't specify if the ground terminals are internally connected.
Product line
ION8600/8650
Resolution
*Warning: Installation and maintenance of this device should only be performed by qualified, competent personnel that have appropriate training and experience with high voltage and current devices. Failure to follow the instructions / warnings in the Meter Installation Guide can result in permanent damage to the meter, severe injury or death.*
The ION 8600/8650 ground terminal is connected internally to the auxiliary power supply's ground terminal. However, to meet electrical safety standards, the meter must be installed with an adequate chassis ground connection and the auxiliary ground 'G' terminal must be connected to earth ground.
Released for:Schneider Electric Global