Browse FAQs

How do I set the rotary switches of the BMXNOE0100 to properly assign the IP address?

Published date: 04 November 2019

Issue:
How do I set the rotary switches of the BMXNOE0100 to properly assign the IP address?

Product Line:
M340

Environment:
EcoStruxure Control Expert
Unity Pro

Resolution:
Summary of M340 NOE rotary switch for Valid IP Address Settings
Each rotary switch position that you can use to set a valid IP address is marked on the module.
The following information summarizes the valid address settings:
  • Device name: For a switch-set device name, select a numeric value from 00 to 159. You can use both switches
  • On the upper switch (Tens digit), the available settings are 0 to 15
  • On the lower switch (Ones digit), the available settings are 0 to 9
  • The selection on the lower switch of any non-numeric (BOOTP, STORED, CLEAR IP,DISABLED) makes the setting on the upper switch inconsequential
  • BOOTP: To get an IP address from a BOOTP server, select either of the two BOOTP positions on the bottom switch
  • STORED: The device uses the application’s configured (stored) parameters
  • CLEAR IP: The device uses the default IP parameters
  • DISABLED: The device does not respond to communications.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.