{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How to simulate a fault condition on an ATS22 or ATS48 soft starter to verify the fault status circuitry is working properly?
Issue:
How can I simulate a fault condition on my ATS22 or ATS48 soft starter to verify my fault status circuitry connected to the starter is working properly?

Product line:
ATS22 and ATS48 series soft starters

Environment:
All models, All serial numbers

Cause:
Customer needs to generate a fault condition on the starter in order to verity their building management system registers the fault properly.

Resolution:
An easy way to generate a fault on an ATS22 or ATS48 series starter is to provide a run command to the starter when the motor is not connected.  The ATS22 will display SCCR and the ATS48 will display PHF.  Any relays assigned to a fault function will actuate.

Schneider Electric Global