How do you configure an ATV61 or ATV71 series drive to trigger a freewheel stop via a logic input terminal?
Published date:
13 February 2019
Issue:
How do I configure an ATV61 or ATV71 series drive to trigger a freewheel stop via a logic input terminal?
Product Line:
Altivar 61, Altivar 71 series.
Environment:
All models, All serial numbers
Cause
Need to configure a logic input, separate from the run command, to stop the drive if an external event is triggered.
Resolution:
From the main menu, set your access level to either Advanced or Expert. If your access level is not Advanced or Expert, you will not have access to the parameters necessary to create this function.
From the main menu, navigate to the drive menu and then to menu 1.7, Application Function. Press enter here and scroll down to Stop Configuration and press Enter. Scroll down to Freewheel Stop Assignment and press enter. Select the logic input you wish to use to trigger the freewheel stop function and press enter.
Freewheel stop is an active low function, so once a logic input is assigned to this function, the function will be acting any time +24V is NOT present on that logic input (in source mode) and anytime the logic input is not connected to common (In sink mode). Factory default mode for the drive is Source mode and it requires a physical switch on the terminal interface card be moved to switch to sink mode.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.