Can you use an external +24V on the ATV58 to power up the control board?
Published date:
08 November 2018
Issue:
Can you use an external +24V on the ATV58 to power up the control board?
Product Line:
Altivar 58
Environment:
All models and serial numbers
Cause:
None
Resolution:
An external +24V power cannot be used to power on the control board of an ATV58 drive. The ATV58 generates its own +24v from the line voltage for use with the control circuits.
An external power +24v power supply can be used instead of the internal to control the drive (not power it up) if the common external supply is tied to the COM terminal. The external +24 and internal +24 must be isolated.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.