{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
OFS / Windows Operating System Compatibility
OFS V3.50 is compatible with the following Windows platforms (2000, XP, Vista, Server 2003, 7, Server 2008, Server 2008 R2, 8, Server 2012).

Up to OFS V3.34, OFS is compatible with Windows 32 bits only.
From OFS V3.35, OFS is compatible with Windows 64 bits including Windows 7.
From OFS V3.40, OFS is compatible with Windows Server 2008 and Windows Server 2008 R2.
From OFS V3.50, OFS is compatible with Windows 8 and Windows Server 2012.
From OFS V3.60, OFS is compatible with Windows 10, Windows Server 2012 R2
From OFS V3.62, OFS is compatible with Windows Server 2016
From OFS V3.63, OFS is compatible with Windows Server 2019
From OFS V3.63 SP2, OFS is compatible with Windows 11
From OFS V3.63 SP2, OFS is compatible with Windows Server 2022

Note : OFS is supposed to follow the evolution of the Operating System.

Schneider Electric Global