{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Why isn't my controller taking the IP Address assigned to it in my SoMachine 4.1 project?
Issue
Controller not taking IP Address

Product Line
SoMachine

Resolution
The most common reason why the IP Address is not assigned to the controller is because the controller already has a Post Configuration loaded. To load a new IP Address to the controller there are two options. One option is to reload the firmware on the controller with a post configuration or you can Process the Communication Settings in SoMachine. You must right-click on the controller and select Process Communication Settings. This will send another post configuration to the controller.

img1

Schneider Electric Global