What is the master password for the ATV61 and ATV71 drives?
Published date:
21 November 2019
Issue:
What is the master password for the ATV61 and ATV71 drives?
Product Line:
Altivar ATV61 and ATV71 drives
Environment:
All
Cause:
Customer does not know the password and would like to bypass it to make a simple programming change
Resolution:
There are two pin codes that can be set on the ATV61 and ATV71 drives.
From the Main Menu scroll down to 'Password' and press Enter
Pin code 1 password reset is 6969
Pin code 2 password reset is 2663
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.