{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Are braking resistors available for the ATV12 drives?
Issue:
ATV12 breaking resistors available

Product Line:
Altivar 12

Environment:
All models and serial numbers

Cause:
None

Resolution:
The ATV12 drives do not have built in braking units so an external braking module is required.
In the USA, braking module VW3A11701 can be connected to the drive and the braking resistor can then be connected to the braking module.
Powerohm is a 3rd party vendor that Schneider Electric in the USA has partnered with to provide DB resistors, since some resistors in our Global documents are not released for sale here.
For specific DB Resistor selection, feel free to contact Powerohm at 800-838-4694.

Schneider Electric Global