{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What can I do if SoMachine Basic cannot establish connection with the PLC TM221 after have updated it with the firmware 1.3.2.1 SP1
This issue can be solved downloading any application in the PLC TM221 via USB in power less mode ( no power supply connected )
After that the issue will not appear anymore

Schneider Electric Global

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: