Browse FAQs

What parts are included in the VW3L10111 Installation Kit for Lexium Integrated Drives?

Published date: 03 October 2018

The kit consists of the following components.

2 - Cable Entries
1 - Molex connector for CN1   (supply voltage)
1 - Molex connector for CN2   (field bus connection)
1 - Molex connector for CN3   (CAN / RS485 interface)
1 - Molex connector for CN4   (I/O signals)
1 - Molex connector for CN5   (STO signals)
Also including enough crimp contacts for all connectors and associated hardware for Cable Entry strain relief

Attached is an image of the complete hardware set found in VW3L10111


Rev 10-3-18
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.