Browse FAQs

How do you go from 3 wire control to 2 wire control on the ATV312 drives?

Published date: 21 January 2020

Issue:
Looking to go from 3 wire control to 2 wire control, on the ATV312 drives.

Product Line:
Altivar ATV31 and ATV312 drives

Environment:
All

Cause:
The drive was programmed for 3 wire control and now they want change it to 2 wire control.

Resolution:
Programming changes
Go In to the IO menu enter.
find TCC enter
If TCC is 3 C change it to 2C for 2 wire control,
Please note this is a special parameter you will need to hold enter for 3 to 4 seconds.


 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.