Browse FAQs

Osisense XC_What is the ZCKY45 lever?

Published date: 30 August 2019

1) ZCKY45 lever is the variable length thermoplastic roller lever used in the obsolete XCKP XCKT plastic limit switches, black casing. Attached product picture. ZCKY46 is the same roller lever with steel roller.
2) In 2019, it is still available to order for spare parts.
3) In the current range of XCKP XCKT blue limit switches, plastic case; equivalent lever for this blue range is the ZCY45 lever. Please note that the ZCY45 lever is positive for safety applications, not the old ZCKY45 one.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.