Browse FAQs

Why is there no decimal precision in ION Setup?

Published date: 03 May 2019

Issue 
ION Setup is showing no decimal precision for either the data recorders or the real time data

Product line
ION Setup

Cause 
The regional formatting is set to an non-North American standard for decimal point ( a comma instead of a period) which causes the decimal points to incorrectly be dropped.

Resolution
Upgrade to ION setup V3.0.15233.1 or newer from the link below:
https://www.se.com/ww/en/download/document/ION_Setup_Latest_Release/​
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.