Browse FAQs

What causes FST on the display of the Altivar drives?

Published date: 15 May 2020

Issue: 
FST on the display of the Altivar drives.
 
Product Line:
Altivar 61, Altivar 71, Altivar 312, Altivar 12, Altivar 31, Altivar 58, Altivar 66
 
Environment:
All serial number
 
Cause:
What causes the drive status to show FST?
 
Resolution:
FST is fast stop. This is a status, not a fault.  This status happens if a logic input is assigned to FST and the logic input is active. The second option is when the VFD is in a decelerating state and the type of stop is assigned to fast stop (FST).

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.