Browse FAQs

Can the application on a broken XBTGT be transferred to a new replacement?

Published date: 01 November 2019

Issue:
Magelis XBTGT need to be replaced. Looking for a way to move the application from the old unit to the new unit.

Product Line:
Vijeo Designer (all versions), Magelis HMI series, XBTGT, HMIGTO, HMIGK, HMIGTU, HMISTU, HMISTO

Resolution:
If the Magelis HMI does not have the VDZ file backed up on it (on either the Secondary or Optional drive), then it is not possible to transfer the existing application on the Magelis HMI to a new replacement. If the VDZ is available, then the user may use the VDZ file to download to the new replacement using Vijeo Designer.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.