{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is there any problem if the core especially the upper yoke has a temperature of 120°C even on an idle run in Resiglas dry type transformers?
No,there is no problem if the core especially the upper yoke has a temperature of 120°C even on an idle run in Resiglas dry type transformers .It can even have temperature greater than 120˘C. The maximum permissible temperature of the core is defined only by the temperature withstand parameters of other parts of the transformer. Standard temperature protection for windings (class F) is set on 145° for alarm and 155°C for tripping.

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.