Browse FAQs

Preventa XCS - XCSLF373731M3 pin-out of the M23 connector

Published date: 10 June 2019

Please find attached the wiring diagram of the XCSLF373731M3 safety switch, having 2NC + 1NO main contacts and 2NC + 1NO electromagnet contacts. It is a version with locking by electromagnet on de-energisation, with M23 19-pin connector. The electromagnet contacts are represented electromagnet not energised. This wiring diagram is valid too for the following references :
- XCSLF373741M3
- XCSLF373751M3
- XCSLF373761M3.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.