Browse FAQs

Preventa XCS - XCSLF353531M3 pin-out of the M23 connector

Published date: 10 June 2019

Please find attached the wiring diagram of the XCSLF353531M3 safety switch, having 1NC + 2NO main contacts and 1NC + 2NO electromagnet contacts. It is a version with locking by electromagnet on de-energisation, with M23 19-pin connector. The electromagnet contacts are represented electromagnet not energised. This wiring diagram is valid too for the following references :
- XCSLF353541M3
- XCSLF353551M3
- XCSLF353561M3.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.