{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can the ATV212 be set up for Automatic Restart after a power outage when the drive is in local control mode?

Issue:
Setting  ATV212  for Automatic Restart after a power outage, when the drive is in local control mode.

Product Line:
Altivar ATV212 S-flex Sflex 212 Sflex 21

Environment:
All

Cause:
The drive is not restarting in after a power outage while running in local mode.

Resolution:
The drive will not reset after a power outage when it's in local mode.  You will need to push the Run button again to start the drive.
If you want an automatic restart after a power outage, consider using a 2-wire dry contact for starting on the terminal inputs.

Schneider Electric Global