Preventa XCS - How to order the XCSZC590L01M8 part number ?
Published date:
24 June 2019
Find attached the picture of both part XCSZC1 magnet and XCSZC590L01M8 detector which is not sold in spare parts. Both parts are sold under complete magnetic switch XCSDMC590L01M8. This is the commercial reference to order to get the XCSZC590L01M8 switch with the magnet XCSZC1, sold into the same packaging plastic bag. The following rule can be applied to all XCSDMC magnetic switches : XCSZC1 + XCSZC59* (or XCSZC79*) = XCSDMC59* (or XCSDMC79*) complete magnetic switch; e.g. XCSZC1 + XCSZC5912 = XCSDMC5912 commercial ref.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.