Browse FAQs

Preventa XCS - How to order the XCSZP7012 part number ?

Published date: 05 June 2019

Find attached the picture of both part XCSZP1 magnet and XCSZP7012 detector which is not sold in spare parts. Both parts are sold under complete magnetic switch XCSDMP7012. This is the commercial reference to order to get the XCSZP7012 switch with the magnet XCSZP1, sold into the same packaging plastic bag. The following rule can be applied to all XCSDMP magnetic switches : XCSZP1 + XCSZP59* (or XCSZP79* or XCSZP50* or XCSZP70*) = XCSDMP59* (or XCSDMP79* or XCSDMP50* or XCSDMP70*) complete magnetic switch; e.g. XCSZP1 + XCSZP5012 = XCSDMP5012 commercial ref.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.