Search FAQs
Safety limit switches XCS - How to order the XCSZR5912 part number ?
Find attached the picture of both part XCSZR1 magnet and XCSZR5912 detector which is not sold in spare parts. Both parts are sold under complete magnetic switch XCSDMR5912. This is the commercial reference to order to get the XCSZR5912 switch with the magnet XCSZR1, sold into the same packaging plastic bag. The following rule can be applied to all XCSDMR magnetic switches : XCSZR1 + XCSZR59* (or XCSZR79*) = XCSDMR59* (or XCSDMR79*) complete magnetic switch; e.g. XCSZR1 + XCSZR7902 = XCSDMR7902 commercial ref.
Released for:Schneider Electric Global
Attachment(s)
Explore more
Explore more